|
Legrand / Raritan / Server Technology Xerus™ JSON-RPC API
|
Classes | |
| interface | Channel |
| The channel interface. More... | |
| struct | Controls |
| Controls. More... | |
| struct | Format |
| Format. More... | |
| struct | Image |
| Image. More... | |
| struct | ImageMetaData |
| Image meta data. More... | |
| struct | Information |
| Webcam information. More... | |
| struct | Location |
| Location. More... | |
| struct | Settings |
| Webcam settings. More... | |
| interface | StorageManager |
| The storage manager interface. More... | |
| interface | Webcam |
| The webcam interface. More... | |
| struct | WebcamAddedEvent |
| This event is emitted after a webcam was added. More... | |
| struct | WebcamEvent |
| Base type of all webcam event. More... | |
| interface | WebcamManager |
| The webcam manager interface. More... | |
| struct | WebcamRemovedEvent |
| This event is emitted after a webcam has been removed. More... | |
Enumerations | |
| enum | PixelFormat { MJPEG , JPEG , RGB , YUV } |
| PixelFormat. More... | |
| enum | PowerLineFrequency { NOT_SUPPORTED , HZ50 , HZ60 , DISABLED } |
| PowerLineFrequency. More... | |
| enum | Priority { VERY_LOW , LOW , NORMAL , HIGH , VERY_HIGH } |
| Priority. More... | |
Webcam Management.
| enum webcam::PixelFormat |
| Enumerator | |
|---|---|
| MJPEG | Motion JPEG. |
| JPEG | JPEG. |
| RGB | RGB encoded. |
| YUV | YUV encoded. |
Definition at line 12 of file Webcam.idl.
Definition at line 20 of file Webcam.idl.
| enum webcam::Priority |
| Enumerator | |
|---|---|
| VERY_LOW | very low |
| LOW | low |
| NORMAL | normal |
| HIGH | high |
| VERY_HIGH | very high |
Definition at line 15 of file WebcamManager.idl.